Hi,
The calibration time parameters are defined in the `Converter Electrical Characteristics' with respect to number of Clock Cycles. Which clock is this referencing?
In the applications information section (2.4.2), the datasheet says the 'calibration procedure is exactly the same whether there is an input clock present upon power up or if the clock begins some time after'. This suggests that the 1.5 GHz input clock is not required for the calibration cycle.
thanks