Hi !
I'm using two ADS54J60 on my prototype board. The board has worked for 2 weeks flawlessly. But now, one of the ADC is not working. I've found out that all transceivers lanes on this ADC are stuck at 10mV. The other transceiver lanes on the working ADC are 0.332VDC. After the series capacitors on the JESD204B lanes on both ADC, the common-mode voltage is about 0.7VDC. The ADC configuration seems to be valid, I can access the SPI registers. All the power pins are at the nominal levels, the Vcm pin is at 2.1V.
I've checked the TSW54J60 evaluation board and the transceiver lanes are at 0.332VDC at boot-up without any FPGA or ADC configuration.
Is this ADC fried?
Thanks,
Patrice