Hi,
I have been working with the DAC38J84 for some time and for a project I want to bypass the DACPLL. So I followed the datasheet steps as follows:
- reset_pll = 1, pll_sleep = 1
- enable_pll = 0
- serdes_clk_sel = 1
I am feeding the DACCLK input with 500MHz for a 500MSPS conversion rate. The JESD lines work at 5Gbps (8 lanes with 841 configuration and half-rate).
The input frequency at the SERDES PLL is also 500MHz with a MPY factor of 5, thus generating 2.5GHz at the output.
For some reason I can't make it work (the SERDES PLL doesn't lock). However if I use the internal DACPLL, everything is fine.
If I don't put the pll into sleep (pll_sleep = 0), I can get the SERDES PLL to lock, but the JESD links don't start up.
Am I missing anything??
Thanks in advance.