Hello,
We are looking for ADC converters compatible with Xilinx's FPGA. We have found these two evaluation boards: ADS5281EVM (12 bits resolution, 8 channels and 50 MSPS) and ADS5287EVM (10 bits resolution, 8 channels and 65 MSPS). We have read in this documents that these converters have a Serial interface to configure them, and these interface is driven to an USB and controled with a Software running in a PC.
We wondered if there is any way to control these serial interface and these converters only using the FPGA ? . I mean, if is there any way to pass these serial interface´s pins to the FPGA to configure the converters here, without needing to use the USB and the software ?
Thank you.
Sincerely,
Javier Nuñez Sanchez