Other Parts Discussed in Thread: DAC3484
For the DAC3482, the datasheet shows that the I and Q complement in the config1 registers are located at bits 6 and 5.
For our application we need to set both of the I and Q complement bits. However, when we set or clear bit 5 in config1, we see no change in behavior from the Q output.
We do see what appears to be correct behavior if we instead assume the I and Q complement bits are located at bits 7 and 6 and then set both of those bits.
Can you confirm? Is the I complement bit located at bit 7 and the Q complement bit at bit 6 in the config1 register?
Regards,
Paul