Part Number: TSW1400EVM
Hi,
I have TSW1400EVM and was trying to develop my own algorithms to work with ADS5294EVM and DAC3484EVM. To have the debugging option available through JTAG, I have done the following modifications to the boards (courtesy of other questions/answers in the same forum for accessing the JTAG)
install R55, R57, R58, R59, R60 and R129 and remove R61, R62, R63, and R64 and I can access JTAG and program the FPGA. So far so good
Now I am trying to program EPCS64 and not having any luck. I used JTAG indirect programming using .jic file and I get the following message/errors in quartus
Info (209060): Started Programmer operation at Wed Mar 29 11:30:09 2017
Info (209016): Configuring device index 1
Info (209017): Device 1 contains JTAG ID code 0x024200DD
Info (209007): Configuration succeeded -- 1 device(s) configured
Error (209025): Can't recognize silicon ID for device 1
Error (209012): Operation failed
Info (209061): Ended Programmer operation at Wed Mar 29 11:30:20 2017
I am not sure why I can't program EPCS device. Is there a way I can configure EPCS64 by removing and/or installing some other resistors on the board? Please let me know as I am stuck with this
Thanks,
Ramakrishna