This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC37J82: SYNCB P/N DAC37J82

Part Number: DAC37J82

Hi

For DAC37J82, the pins SYNCBP/N are LVDS OUTPUTS. What is the meaning of Zt : internal termination 100oHm ?

I understand this point for LVDS INPUT but about LVDS OUTPUT ...? is 100ohm load ,for LVDS output , in DAC37J82 ??

3 Replies

  • Antoine,

    This may be a typo in the data sheet as this makes no sense to me either. I am checking with the design team regarding this. On our EVM, we treat this as a standard LVDS output with 100 Ohm differential traces connected between these pins and the connector.

    Regards,

    Jim

  • In reply to Jim Seton:

    Jim

    Have you an answer from the design team to confirm about this? There is no resistor 100ohm inside the component between SYNCB+ and SYNCB-

    Best regards 

  • In reply to Antoine Michelangeli:

    Antoine,

    This is an internal termination resistance on the LVDS output.  It double terminates the transmission line at the source end.  The user is still required to terminate the load end of the SYNCB transmission line.  See “config52” for details on the register settings.  There is also control for the output current on the LVDS output in this same register.

    Regards,

    Jim

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.