Part Number: TSW1266EVM
Greetings,
I am trying to use TSW1266 EVM with TSW1400 to acquire a complex modulated signal with "High Speed data Converter Pro" version 4.5. I followed the user manual of TSW1266 EVM which instructs to selec the device "ADS5402" from the drop own menu in the list of ADCs available on HSDC Pro. I couldn't find ADS5402 there and instead selected ADS5401-09 but I couldn't acquire a signal. I loaded the configuration file named "LMK04808_614p4M_Single_Loop.txt". I set my RF input frequency at 2.149GHz (-30dBm) and LO at 2.6GHz (0dBm) as instructed by the user manual.
I am not sure whether the PLL of the clock generator has locked since I don't find the LED 'D1' being lit as specified in the user manual which says "The LED labeled D1 on the board will light up indicating that both PLLs are locked." But I find that the LED 'D3' is lit. LED 'D3' is connected to the Lock Detect pin of LMK04808 as per page 5 of the schematic of TSW1266 EVM.
I am unable to figure out the cause behind failure to acquire any signal at all. I suspect that the cause could be the firmware file that I have selected i.e. ADS5401-09.ini but not sure since I find this one to be the closest match to ADS5402I mounted on TSW1266 EVM among the ini files available. Could anyone kindly advise what could be the problem?
Thanks and Warm Regards,
Prasidh