Other Parts Discussed in Thread: DAC38RF80
Hi,
I want to test the DAC38RF80 in a dual IQ dual DAC mode (the default state supports single IQ dual DAC mode).
In the default mode everything works fine ( including interfacing with the high speed data converter pro).
When i try to configure it to a different state ( using the configuration file 2T2R_RevC_ConstInput_12xDec_24xint_2949p12M_5859p2_2IQ_4915p2Gb.cfg)
i can't manage to output a signal from the DAC, not to mention using the high speed data converter pro.
The label don't update (interpulation, sampling rate, etc)
Could you provide a step by step guideline to configuring the EVM to a mode different from the default one?
Also,
In case i would like to use a different reference frequency at the input to the on chip PLL inside the DAC, do i need to
define different value for the digital/analog delays of sysref in order to meet setup and hold spec?
Thanks in advance,
Guy.