Part Number: TSW14J10EVM
Hello,
I am working with a system that utilizes the KC705, TSW14J10EVM, and ADC32RF45EVM to process an analog system with custom FPGA firmware. I have found that many of the JESD lanes do not actually connect to the FPGA instead they end at the FMC connector on the KC705 board.
I bought this board because it stated compatibility with the KC705 board but it looks like this is not the case. To make sure that I wasn't crazy I looked up the schematic for the VC707 board and sure enough, all the lanes are connected.
If this is truly incompatible, I recommend removing the KC705 board from the list of compatible boards.
Thanks,
Robbie