This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC32RF45EVM: HSDC Pro 4.70 version can't select the ADC tab, and select "ADC32RF34_8224" using the drop-down menu in HSDC Pro With Xilinx® KCU105

Part Number: ADC32RF45EVM
Other Parts Discussed in Thread: ADC32RF45

Hi.

I am designed ADC32RF45EVM  board and KCU105EVM Board.

ADC32RF45EVM With KCU105 Board Setup Example in "HSDC Pro With Xilinx® KCU105 User guide (SLAU711–March 2017)"

Set up the hardware as follows:

1~9 is ok.

but, "10. Open HSDC Pro, select the ADC tab, and select "ADC32RF34_8224" using the drop-down menu" is not supported in HSDC Pro 4.70.

but, i can't see "ADC32RF45_8224" in drop-down menu.

i want to this example completed.

what is problem?

Help me please.