Other Parts Discussed in Thread: LMK04828, , ADS54J66
Hello,
I am using an ADS54J66EVM+TSW14J56EVM for my project. Until now, I have tested my boards under Matlab with an internal clock from the onboard VCXO. I will now use an external clock generated by a DDS card that does not have a 10MHz output for synchronization with the LMK04828. What is the best solution for my configuration? I use the J6 input clock or J12 with JP2 jumper removed? is there any changes to be made on the ADC board or only sotware configuration to do (LMK_Config_External_Clock.cfg) for example.
Best regards
Said FARAH