Hi,
Looking at the manual for the ADS42LB69, section 8.3.1 on digital gain, I'd like to better understand how this feature is implemented. From the manual:
"The device includes gain settings that can be used to obtain improved SFDR performance (compared to no gain)...SFDR improvement is achieved at the expense of SNR; for a 1-dB increase in digital gain, SNR degrades approximately between 0.5 dB and 1 dB (refer to Figure 15 and Figure 16). Therefore, gain can be used as a trade-off between SFDR and SNR. Note that the default gain after reset is 0 dB with a 2.0-VPP full-scale voltage"
Why would increasing digital gain after sampling occurs have any impact on the SNR or SFDR? Is digital gain applied uniformly to all samples or some function of input amplitude? If want to change my input range from 2 Vpp to 1 Vpp I would expect an (analog) amplifier to boost my 1 Vpp signal to 2 Vpp prior to digitization in order to make use of the full 16 bits of the converter. If I apply 6 dB of digital gain, which restricts my input voltage range to 1 Vpp, am I not losing my MSB and hence reducing my theoretical SNR by 6 dB?
Thanks!
-Sean