Part Number: TSW1400EVM
Hello,
does the TSW1400EVM support a sampling of two channels with a sample rate of 500 MSPS each and a bit resolution of 12 Bit like it's necessary for example for the ADS5407. In the desciption I can find that it provides 16-bits of data at 1.5 GSPS. However, in the User's Guide of the TSW1400EVM I found the information "For two-channel parallel DDR bit-wise data formats, 14 of the LVDS data pairs are used to support two channels of 14-bit resolution at up to 250-MHz sampling rate." How do these two informations fit?
Best regards
Benjamin