This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC3482: Operating DAC3482 on non complex signals

Part Number: DAC3482
Other Parts Discussed in Thread: ADS4249,

I got a digital data stream (2's complement format) coming from ADS4249 14 bits ADC at 250 MHz.

Those are actually 2 independent channels (like a 2 oscilloscope channels).

I would like to output this data (Thru FPGA) to DAC3482 and disable the internal complex mixer or any other operation between the data of the 2 channels (i.e. reconstruct the 2 Analog channels that I input to ADS4249) while doing X4 interpolation and taking advantage of the internal SINX/X interpolation with the internal smoothing filters (Fig. 65 in the datasheet). Is it possible to do that?

If I use the DAC in this mode, would it be possible to correct the gain and offset of each channel independently? (Mixer is OFF).

I would appreciate your detailed answer including which registers to set in order to do that.