Hello,
I am using an ADS54J42 ADC on a custom PCB. The ADC sample clock rate is 400 MHz. I'm doing LMFS = 4244. So I get four samples at a time out of my JESD204 receiver at 100 MHz. There is a distinct DC bias between "taps" (tap a sample 0, tap b 0, tap c 0, tap d 0 come out of the JESD204 receiver at the same time). The data is shown below for my two PCBs. The bias seems to remain the same from power-up to power-up but is distinctly different between PCBs. What's wrong? How do I fix it? Thanks.
Units are counts
SN1
mean(a) - mean(b) = 35
mean(a) - mean(c) = -106
mean(a) - mean(d) = -49
SN2
mean(a) - mean(b) = -14
mean(a) - mean(c) = -146
mean(a) - mean(d) = -131