Just received my LDC1000 EVM yesterday, and put it through its paces using the LDC1000 GUI.
Great stuff ! I can see a number of areas in Process Control where this new sensor could be used.
Next step is to actually sit and down and start programming this thing, and hooking it up to other MSP430s and Tiva/Stellaris MCUs to run against some process control hardware. (Thank you for putting in the breakable tab to easily separate the LDC and sensor, and for putting in 0.1" tabs for soldering. I won't have to go blind trying to solder to it !)
Will TI be posting any sample code (initialization sequences, typical usage, ...) and/or the demo software that runs on the EVM's F5528 ?
Sample code would sure save a lot of "re-invention of the wheel" and redundant experimentation vis-a-vis initialize and startup.