Good Afternoon
I have an application where I need to have the LDC1000 coils as close together as possible to read a strip across the topology of a 30cm x 3000cm surface. The approximate range is 3cm and so I have opted for the smallest coil from your design set of 3.71cm diameter. Accuracy is not particularly an issue.
Given only one coil is being powered at a time and I waiting 3 cycles before reading, what is a safe distance between coils so they don't interfere? Can they be adjacent? If they all have at least one non-active coil immediately adjacent, can I calibrate the surrounding non-active coils out of the reading?
Any suggestions at all would be gratefully appreciated.
Thanks
Jonathan