Hi! I'm going to use the LDC evm (I had it already) like a wear debris sensor. I want to register small wear debris in fluid flow. I suppose the fluid with debris will flows through L-tank (in plastic tube, for example). The velocity of flow is around 2 m/s. The diameter of debris is around 50um and larger. Also I hope, that I can to determine a material of debris (magnetic/ nonmagnetic for example).
Do you think it's really?