There seems to be some strange behaviour on the start samples of each datablock when using New firmware and command "06". The data is normal when reverting back to old firmware using firmware linked in the post "LDC1000 EVM GUI 1_0_4_1"
The problem is that there is a jump in sample value for both type of samples.
I first thought the jump was between the Blocks, but the jump is from first sample in the block to the next sample.
Here is a Picture of 1520 samples of Frequency Counter
Next Picture is a closeup of samples round sample 512. Samplecount start at 0.
The last Picture is Reading With old firmware.
No jumps With old firmware so the sampleperiod is not corrupt for first to samples in Block.
I have reverted to old firmware and that has the needed functionality for my Applications.
I Guess this do not affect New GUI as it no longer read 2k Blocks.
Kind regards
Torgeir Skomedal
Here is a greeting from Norway
LDC1000EVM , coil about 1mm from speakerdiagraph. Heavy eq.