As stated in the subject, The method I have tried is to use the device manager to update the device driver. But after I selected the driver folder (that contains the driver for the LDC1000EVM) it returns that "Windows couldn't find driver software for your device". Have anyone else encountered this problems?
I also tried to use the MATLAB (on OS X) interface but couldn't locate the com port where the devise where attached and thus couldn't communicated with the LDC1000EVM.
I have searched the interweb for different ways to force install drivers and also fusion 6 forums for similar problems. I think that maybe the problem could be that the device name doesn't propagate from the macbook to the VM and that the device driver is connected to the intended hardware with some kind of name. Also tried to change the code in the driver but i couldn't affect that. And also i don't have any experience with driver-programming.
The device is known as "texas instrument input device" in the macbook, but only "unknown device" in the windows VM.
Any help would be most welcome. Sorry for this long question.