Hi,
I downloaded the GUI update to enable data logging and I am finding that the the the data will accumulate for up to two hours before the data collection hangs and the last data point is displayed continuously. I have tried the EVM on two PCs with the same result. My question is are the parameters I am using within the capability of the EVM? I have reduced sampling frequency to once every sixteen seconds so that I data log over an extended period of time. My basic setup parameters are as follows:
Capacitor 100pF
LDCLK 6MHz
Samples 550
uC sampling rate 0,0625Hz, 16 secs
Mode is single point saved to log file in continuous mode.
Many thanks for your advice.
Dave