Can I use a unsheilded inductor (normally used with DCDC converters) with the LDC1000?
Can I use RFID coil with the LDC1000?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Hithesh
Yes, un-shielded SMT inductors can be used with LDC1000. Please note that the sensing range is relatively closer with most SMT inductors.
As for RFID, as long as the inductance is suitable, they can be used with LDC1000
Don