Please let me know two points below about output register and Rp_max of LDC1000 and LDC1051.
・Is a LDC output register a maximum of 8bits(255)?
Although outputted only to 7bits(128), what is reasonable ?
・Rp_max is set as the maximum.
(Address 0x01 set 0x00:3926.991kΩ)
When LDC output becomes the same as Rp_max, is there any problem?
(Is a problem in the output of INTB?)
Best regards,
Satoshi