I set the LDC1000EVM parameter as follows.
Rp max = 3078 ohm
Rp min = 1796 ohm
f sensor = 2688.820 kHz
I get the log data with the default sampling frequency = 1kHz all right.
But, when I set the uC Sampling Rate to 10kHz, I got the same data 6 to 12 times in the log file.
As I measure the rotaing smooth surface rotar, the value shoud change continuously.
Please tell me how to set the uC Sampling Rate which truely measure the inductance at that sample rate, not repeating the same data several times.
By the way, Is it possible to set uC Sampling Rate at 70 kHz maximum with the LDC1000EVM and GUI software?
part of the log_data_file
04:09:14:13:39:55:273.600 27601 139.6 13.787 uH 27601 3511
04:09:14:13:39:55:273.700 27601 139.7 13.787 uH 27601 3511
04:09:14:13:39:55:273.800 27601 139.8 13.787 uH 27601 3511
04:09:14:13:39:55:273.900 27601 139.9 13.787 uH 27601 3511
04:09:14:13:39:55:273.000 27601 140 13.787 uH 27601 3511
04:09:14:13:39:55:274.100 27601 140.1 13.787 uH 27601 3511
04:09:14:13:39:55:274.200 27677 140.2 13.787 uH 27677 3511
04:09:14:13:39:55:274.300 27677 140.3 13.787 uH 27677 3511
04:09:14:13:39:55:274.400 27677 140.4 13.787 uH 27677 3511
04:09:14:13:39:55:274.500 27677 140.5 13.787 uH 27677 3511
04:09:14:13:39:55:274.600 27677 140.6 13.787 uH 27677 3511
04:09:14:13:39:55:274.700 27677 140.7 13.787 uH 27677 3511
04:09:14:13:39:55:274.800 27717 140.8 13.803 uH 27717 3513
04:09:14:13:39:55:274.900 27717 140.9 13.803 uH 27717 3513
04:09:14:13:39:55:274.000 27717 141 13.803 uH 27717 3513
04:09:14:13:39:55:275.100 27717 141.1 13.803 uH 27717 3513
04:09:14:13:39:55:275.200 27717 141.2 13.803 uH 27717 3513
04:09:14:13:39:55:275.300 27717 141.3 13.803 uH 27717 3513
04:09:14:13:39:55:275.400 27660 141.4 13.866 uH 27660 3521
04:09:14:13:39:55:275.500 27660 141.5 13.866 uH 27660 3521
04:09:14:13:39:55:275.600 27660 141.6 13.866 uH 27660 3521
04:09:14:13:39:55:275.700 27660 141.7 13.866 uH 27660 3521
04:09:14:13:39:55:275.800 27660 141.8 13.866 uH 27660 3521
04:09:14:13:39:55:275.900 27660 141.9 13.866 uH 27660 3521
04:09:14:13:39:55:275.000 27484 142 13.976 uH 27484 3535
04:09:14:13:39:55:276.100 27484 142.1 13.976 uH 27484 3535
04:09:14:13:39:55:276.200 27484 142.2 13.976 uH 27484 3535
04:09:14:13:39:55:276.300 27484 142.3 13.976 uH 27484 3535
04:09:14:13:39:55:276.400 27484 142.4 13.976 uH 27484 3535
Hope to get any help soon!