Dear TI FAE,
I have a question. I wonder whether it is possible to use "Wire to Board Connector" or not.
The sensor is not PCB coil, but a discrete component. And it is NOT possible to mount it on the PCB.
It is necessary to use wire cable, like shielded or coaxial.
So, I'm trying to use "Wire to Board Connector". But I'm affraid that the impedance would be changed
due to the connector .
Have you ever heard the application examples such like this?
In my system, the sensor frequency or LDC1000 is about 40kHz.
It is similar to auditory bandwidth...
Kindest Regards,
Edgard