I have created my own coil in a ferrite core and connected it to the LDC1000evm with a 20000pf cap. It works good but I am trying to get a good sensitivity on this so that it will detect a .003" change in distance. I am using the GUI to see what it is doing and sometimes it changes within .003" and other times around .04". Is there something I need to do to get the sensitivity better?
My coil is hand wound with 200 turns and is .68" od.