Hello,
We purchased the ADS1298RECG-pdk evaluation development kit and noticed that an executable(ADS1298e.exe)came with it. Additionally, itwould seem that the executable was developed from labview.
I looked into the folder where the application is installed and notice that there are VIs located throughout the installed folder. I have triedto match the ADS1298E.exe's GUI application with the accompanied Vis and wasn'table to do so.
Are the ADS1298E.exe's VIs located in the extracted folder and if so can what are their file names?
If not can where can I get the VIs that were used to create the ADS1298.exe.
Thanks Very Much.
--cat--
On it's way, good luck!
-------------------------------------- Kevin Duke Precision DAC Applications
Hi Kevin
I'm Pedro. Could you send me the password for source code too?
Thanks
PD: my mail is.... gamboaxx@gmail.com
Hi Kevin,
I guess I am a little late to the party. Please send me the password to the firmware and labview zip files. I purchased a ADS1298R EVM kit. Thank you very much.
-- Mike
On it's way, enjoy!
I AM A STUDENT DOING A THESIS ABOUT ECG SIGNALS WORKING WITH THE ADS1298ECG.FE.PDK MY PROBLEM IS: ADS1298 HAS A SOFTWARE DEVELOPED IN LABVIEW. AS IT WAS DEVELOPED IN LABVIEW, I NEED TO KNOW IF THE ADS EVM SOFTWARE HAS A VIRTUAL INSTRUMENT SO I CAN PROCESS THE ECG SIGNAL USING LABVIEW IN A DIFFERENT Virtual Intstrument.
I would like to have the password so I can manipulate the information of the signal captured by the ADS1298ECG.FE.PDK
thank you for any help you can give me
Martin
Hi Martin,
Welcome to the E2E community. The ADS1298ECG-FE software is a virtual instrument. The source provides you with the front-panel VI, all of the supporting VIs, and a LabVIEW project containing everything in an organized fashion. You could modify or add additional signal processing in the front-panel VI. I'll be sending you an email with the password soon. If you have any further questions you're welcome to ask, but the software is unsupported for the most part unless you have a very specific question.
Good luck in your project!
Martin -
Kevin will send you information on the source code. However, I wanted to offer that the software does NOT have a virtual instrument for use in other VIs. The ADS1298ECG-FE software is designed as a stand-alone app, and while you can reuse functions and subVIs from the code we will provide, there are not virtual instruments or VIs that you can use in your own VIs to control or collect data. These would need to be developed on your own or obtained by modifying the existing code.
Greg Hupp
Hardware and Software Platform Development
Precision Data Converters
Could you send me the password as well.
Best Regards
Hubert Zhang
Haunqian -
Can you send me your email by "Starting a conversation"? This way you do not have to publicly post your email.
can you please send me the password as well !!
kind regards,
Sebastian
Sebastian -
Either post your email address or start a conversation with either Kevin or myself (and then send email address). We will get the information to you when we receive the information.
Hi Greg,
I've recently acquired the ADS1298RECGFE-PDK. Could you please send me the password for the Labview source code?
My email: ernesto.serrano@upc.edu
Thanks!
Ernesto.
Ernesto -
You will receive an email shortly with the requested information.
Hi Mr. Duke,
I was wondering if i could get that password as well.
Thanks,
David
Sure. Info is on it's way to you.