This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1291 general questions

Hello again ;

 

I need to finish my  design but I need some technical supports as possible as you can and thank you in advanced.

Our design depends on ADS1291 to detect  ECG signals and classify them . We would use only 2 leads there is no RLD lead . But I still need support with some issues.

1. I would use DC leadoff detection but I am using only two leads electrodes , so I cant block DC , what do you suggest a solution ?

2.  I Have to measure the impedence of the body (resistive)  the imperence between the two electrodes I could not find anything about this in the datasheet; please could you explain how to acheive that.

3. I have to detect PACEMAKER activities; hardware detection would be better but also could you suggest an example circuit to be added to ADS1291 ; know that i am using unipolar power supply (0-3.3v).If not hardware any example for software detection ?

4.Does anyone have an opensource ECG classification algorithm?

Thank you inadvanced

Hector

--------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

Note:

This is a team account ; not a personal account. 

11 Replies

  • In reply to HECTOR:

    New Issue ;

     

    I am trying to read the ECG again and again ; as I told the reading are ok ; but there always an offset voltage added to the signal and this offset voltage not fix to subtract it each time ; some times it about 0.01V somtimes it goes to negative  , Do you suggest a solution ?

    Should a pull up resistors to AVDD to the inputs helps to make this offset fix ?

     

     

    --------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

    Note:

    This is a team account ; not a personal account. 

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.