ADS1292R: Respiration and ECG Data Rate Problem

Part Number: ADS1292R

Hi, 

I've continued Laura Cupic's work on interfacing ADS1292R with TM4C123GH6PZ microcontroller:

I've succesfully interface microcontroller with ADS1292R, but the problem occurs when the Data Rate is changed comparing from 125SPS to 8kSPS. 

ADS1292R register values:

CONFIG2   -> 0xA0 (reference buffer enabled)

LOFF          -> 0x10 (lead-off disabled)

CH1SET     -> 0x60 (CH1 enabled, gain 12)

CH2SET     -> 0x60 (CH2 enabled, gain 12)

RLDSENS  -> 0x2F (chop freq=fmod/16, RLD enabled, RLD inputs from CH1 and CH2)

LOFFSENS-> 0x00 (default)

RESP1       -> 0xEA (resp mod/demod enabled, phase 112.5, internal clock)

RESP2       -> 0x03 (32kHz freq, internal reference voltage)

Signal acquisition: simulator -> ADS1292R -> TM4C123GH6PZ (SPI, SCLK = 1MHz ) -> Laptop (UART, Baud Rate=115200)

Respiration signal and ECG are acquired from simulator (LA, RA, LL and RL), Respiration rate is set to 15 per minute (0.25 Hz), so for the Data Rate of 125SPS, 1000 samples equals to 2 periods of respiration signal as shown on the image. Math is correct for 250SPS (2000 samples), 500SPS (4000 samples) but higher than that number of samples sticks to around 4200 for any higher data rate. Same is for CH2 (ECG).

Questions:

1)  Why is number of samples locked for frequencies higher than 500SPS?

2) Why higher frequencies have more noise?

4 Replies

  • Hello Tin,

    Thank you for your interest in the ADS1292R and welcome to the forums!

    1) The number of samples is not locked. Where are you saving this data to? Perhaps it is reaching its limit.
    1a) Page 32. of the datasheet covers continuous conversion mode. Is it possible that your start pin is being toggled low or the stop code is being transmitted?
    1b) Another test to try would be to let a lower sampling rate test run for longer to confirm that it the device stops capturing data after 4200 samples.

    2) There is more noise at higher sampling rates because as the sampling rate increases the oversampling rate decreases. The CONFIG2 register shows the relationship between oversampling ratio and sampling rate. Table 4. shows the relationship between sampling rate and noise-free bits. As the sampling rate increases, the number of output bits that are compromised by noise increases as well.

    Best regards,

    Alex Smith
    Applications Engineer | Precision Delta-Sigma Converters

    Check out our helpful resources:
    TI Precision Data Converters | TI Precision Labs - ADCs | Analog Engineer's Calculator Data Converters Learning Center | Selection Guide

  • In reply to Alexander Smith:

    Hello Alexander,

    Thank you for the quick response and welcoming me to the forums.

    1) I've wrongly expressed what the actual problem was. In the graphs on attached picture, I've cut manually number of samples to show exactly 2 periods od respiration signal. I'm able to get more samples if I transfer data for longer period of time. For example samples used for the attached picture were cut down from data around 15 seconds long. This is plotted data for 125SPS data rate I have recorded from respiration simulator for around 15 sec from where I've cut manually 2 periods for the picture in prevous post:

    Problem is with data rates higher than 500SPS.

    Variables 'file1' to 'file7' are from workspace in Matlab derived from function dlmread that reads data from .txt files. 'file1' is for 125SPS, 'file2' for 250SPS, etc. For every data rate, data is recored around 15 sec, so the number of rows in the variables 'file' that represents number of samples has to double if the data rate is doubled. 

    15s/8ms = 1875 samples for 125SPS, 15s/4ms=3750 samples for 250SPS, etc.

    That is true for data rates 125, 250 and 500SPS. But for higher data rates, for example 2kSPS: 15s/1ms=15000 samples and I get 7764 samples. It seems that max data rate I can get from device is around 516SPS according to number of recorded samples.

    2) Thank you for pointing me to Table 4. The number of compromised bits seems to increase as the higher data rate is chosen no matter to problem 1).

    I hope I've clarified what the actual problem is.

  • In reply to Tin Cvox:

    Happy to help and thank you for clarifying!

    My current thought is that this is a data storage buffer problem. Perhaps wherever you are storing data to is filling up faster than it can empty. I would suggest looking further into this. What software are you using to collect the data?

    The next step is to take a look at your digital SPI pins:

    1) Are you in RDATAC or RDATA mode? This will help us understand if your samples are being corrupted or if they are being missed.

    2) Probe your SPI pins to make sure that when DRDY toggles that there is enough time for CS to go low and SCLK to send 72 clocks (24 status + 2channels * 24 bits) before DRDY signals that another sample is available. Your previous post said that your SCLK is running at 1MHz which should be plenty fast to take the data, but take a look to make sure that your routine doesn't have an issue that is causing you to corrupt or miss samples.

    Best regards,

    Alex Smith
    Applications Engineer | Precision Delta-Sigma Converters

    Check out our helpful resources:
    TI Precision Data Converters | TI Precision Labs - ADCs | Analog Engineer's Calculator Data Converters Learning Center | Selection Guide

  • In reply to Alexander Smith:

    I'm also suspecting that it is data storage problem.

    1)I'm using RDATAC mode

    These are my main.c and ADS1292R.c

    main.cpp

    3554.ADS1292R.c

    For data transmission I'm using UART2 pins on TM4C123GH6PZ connected to UART-USB bridge and for writing to .txt file Putty configured for 115200 baud rate.

    Could you verify if my code is causing this problem?

    Thanks