• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Data Converters » Precision Data Converters » Precision Data Converters Forum » ADS8361 mode IV with DMA
Share
Precision Data Converters
  • Forum
  • Files
  • E2E Wiki
Options
  • Subscribe via RSS
Check out
The Signal blog
  • $core_v2_blog.Current.Name

    Handy Gadgets and Resistor Divider Calculations

    Posted 7 days ago
    by Bruce Trump
    Handy gadgets make our engineering life easier—the little...
  • $core_v2_blog.Current.Name

    Chopper Op Amps—are they really noisy?

    Posted 14 days ago
    by Bruce Trump
    Chopper op amps offer very low offset voltage and dramatically...
  • $core_v2_blog.Current.Name

    Bypass Capacitors… yes, but why?

    Posted 27 days ago
    by Bruce Trump
    Everyone knows that op amps should have power supply bypass capacitors...

ADS8361 mode IV with DMA

ADS8361 mode IV with DMA

This question is answered
Alberto Biancalana
Posted by Alberto Biancalana
on Apr 13 2012 13:10 PM
Intellectual380 points
Hi, I'm planning to use ADS8361 for a 4 channel FSK-FH decoder, using 6418EVM, 5-6k interface board andADS8361EVM.
I want to use mode IV operation of ADS8361, and have the 4 channels 16 bit samples written by DMA on a memory page in interleaved fashion, being sure to associate channels and memory locations.

I read the full documentation of 8631 and also the application note for C6711 (which should be good also for 6418), where MCBSp is configured to receive 20 bit frames with 2 byte delay and a single 16 bit word, but I don't understand a basic thing.

How can I start ADS8361 operations getting samples starting from the first of the 4 channels? and stop operations at any time and then restart again getting samples starting from the first channel?

Should I drive M0 low, generate one or some CONVST/RD pulses with MBsp, stop sending pulses, then drive M0 high, initialize DMA and start MCBsp running?. And do all this after I've stopped and I need to start again?
M0 can't be driven by the EVM using ADS8361 EVM, so should I wire to some GPIO to do this?
Or I should do some other way?
Sorry for the long question, I was not able to explain with less details.
Any help is really appreciated.
Alberto
Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • Tom Hendrick
    Posted by Tom Hendrick
    on Apr 14 2012 08:46 AM
    Verified Answer
    Verified by Alberto Biancalana
    Guru86200 points

    Hi Alberto,

    This sounds like a very interesting project to use the ADS8361 with!  One thing that is not made very clear in the ADS8361 data sheet is that the device starts off from power up in Mode 1.  There is another application note here http://www.ti.com/lit/an/slaa167/slaa167.pdf which you might find helpful.  That document was written for the F2000 series DSP's but it goes into more detail and includes a few scope shots that may help you realize a method to get your project running.

    Figure 4 in the application note mentioned above shows how you can drive M0 low via GPIO and force the ADS8361 into a synchronized state that allows you to simply read the 16-bit conversion results and store the data by CHA0, CHB0, CHA1, CHB1...  The alternative to this is to take all 18-bits from the ADS8361 SDOA (2 CH ID bits + 16-data bits) and sort the data based on the status of the channel ID bits; 00 is A0, 01 is B0, 10 is A1 and 11 is B1.  See Figure 13 in the ADS8361 data sheet for details and note that the first sample should be discarded (this is Mode 1 from power-up).

     

    Regards,

    Tom

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Alberto Biancalana
    Posted by Alberto Biancalana
    on Apr 15 2012 14:24 PM
    Verified Answer
    Verified by Tom Hendrick
    Intellectual380 points

    Thanks Tom, the F2000 document gives much more infos.  I'll find a way to bring a GPIO signal of 6414EVM to the 8361EVM to drive M0 as required.

    Can I ask about a last doubt on 8361?
    This is probably a stupid question that you already answered in your post, but I'm a careful guy since I have very short time to setup this work.
    All the characteristics of 8631 are ok for my 4 channel FSK modem utilization, like sampling rate, resolution, aperture, noise and so on.
    Anyway, I see that in the 8361 datasheet the only suggested application are motor control and others, all of which are out of my knowledge, but not data acquisition or communications.  I think that those are simply suggested applications, also due to the simultaneous sampling feature, but there can be any parameter or reason that escapes me for which 8361 could non fit applications different by the suggested ones, like the one I need?
    Thanks and best regards
    Alberto
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Tom Hendrick
    Posted by Tom Hendrick
    on Apr 21 2012 15:52 PM
    Verified Answer
    Verified by Alberto Biancalana
    Guru86200 points

    Hi Alberto,

    My apologies for the slow response here - the ADS8361 was designed for use with applications that require simultaneous sampling.  The thought was customers who are trying to measure two phase currents, or the output of a sinusoidal encoder in a motor control application would find the interface 'easy' to use while incorporating the ability to capture two distinct signals at the same time.  That being said, there is absolutely nothing about the part that makes it specific exclusive to a motor control application.  Anywhere you need a multi-channel, high speed, high resolution ADC, the ADS8361 would definitely be an appropriate solution.

     

    Regards,

    Tom

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Alberto Biancalana
    Posted by Alberto Biancalana
    on Apr 22 2012 07:20 AM
    Intellectual380 points

    Absolutely no problem for the time, Tom,  and thanks again you for your support.

    I just submitted the project concept based on ADS8361, 5-6K Interface Board, and 6418EVM, and now is coming time of develop SW to test the system.

    Thanks so much

    Alberto


    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use