Hi team I have a customer with a problem on device LMP91000, He can't read or write into registers.
I think what the Status Register is 0, because in the datasheet pag.14, is wrote:
STATUS -- Status Register (address 0x00) The status bit is an indication of the LMP91000's power-on status. If its readback is “0”, the LMP91000 is not ready to accept other I2C commands.
This Register for Default is = 0, now , how can I set the Status register at 1 ?...
Thank a lot.
Pierluigi Rossetti