I am using the TI sigma-delta ADC ADS1178 with my C6747 board. There are some problems i don't understand about the sigma-delta AD ADS1178? would you pls give me some advices?
1. The group delay and settling time in the ADS1178 datasheet page 3 is 38/fData and 76/fData? What does the fData mean? Does it mean the sampling rate? If so, I am gona to sample the data with 8k, and so the group delay is 38/8k>4ms, the settling time is 76/8k >9ms? How does the chip adapt to the industrial control system with such a long group delay and settling time?
2. What are the occasions where the sigma-delta ADCs are suitable? In the real-time control system, the long group delay will limit the wide use of the sigma-delta ADC. I am puzzled that how to use this kind of ADCs? In my system, a timer is used to generate the 1/8k period interrupt, and in the ISR program, read back the AD sampling data, handling the AD data with function program and then output the handled data with DA. How can I use the ADS1178 in my system? Bye the way, ADS1178 works in high-speed mode, TDM data transfer with EDMA..
3. What is the usage of pin SYNC signal in ADS1178? From the datasheet, it can be synchronized by pulsing the SYNC to low and return to high again. In SPI mode, the time for new data to be ready is 176/fData(if fData is 52k, there will be almost 3ms delay). If the SYNC pin is connected to a reference time pulse with 1/8k, will the ADS1178 work properly(that is sample at an interval of 1/8k)?