Hello!
I'm Working on a project about Holter monitor using ADS1293 and I have some questions and I think this is the best place to ask them.
first of all I want to use a '28-pin plcc to dip adapter' for ADS1293 to make it possible to use it on bread board,so the question here is that: is it safe to do it or it will be dangerous for ADS1293? because in datasheet is writing "The leads should be shorted together or the device placed in conductive foam during storage or handling to prevent electrostatic damage to the MOS gates."
the second question is about filters.ADS1293 has programmable low-pass filters,but should I design some High-pass filters for preventing DC voltage?
the third question is about input resistance.Should I put a resistant between lead and ADS1293 channel inputs for protection?
I want to use LPC1768 Cortex-M3 Header Board to program the ADS1293 and read data from it. Is it ok?
the reasons for choosing LPC1768 Cortex-M3 Header Board are availability and being able to use on bread board.
I've searched the forum and read previous topics about ADS1293,and I'll be happy if some one answer my questions and give me some schematics and source codes for my project.
regards
Tom