Hi,
We are currently trying to design an ECG with the INA333, and some OPA2333.
We tried several schematics on breadboards, with 2 and 3 electrodes to acquire the heart rate (more electrodes just can't do for our project). The problem is : we are limited to a single power supply of 3.3V max. Even though we found quite a few schematics of ECGs with different designs, whether on the datasheets or on forums, none of them worked. Moreover, they were mostly designed for a power supply over 5V.
Would someone happen to have a good idea or a schematic that will do the trick please ?
Thanks a bunch !
Cheers