Hello!
Do anybody have made experiences in measuring heart rate with the ADS1298 and capacitive electrodes??
I want to design a input stage with impedance converters and then fed this signal into one channel of the ADS1298.
Is it possible to fed in the signal directly after the impedance converter without the normal input stage which is recommended for the ADS1298?
kind regards
Sebastian