I bought a pre-built ADS1256 board from Aliexpress.com. I hooked it up to an IOIO OTG via SPI but could only get garbage data from it. I then hooked up a logic analyser and confirmed that my SPI signals going in to the ADC are correct.
I then noticed that the ADC is outputting a single 2 or 4 us pulse every 32us. The data-ready pin seems to have worked correctly in response to SPI commands, but the data-out never changes. I have done SDATAC as well. Is this chip faulty perhaps?