Helllo Sir/Madam,
We are using below ADC interfaces:
ADC = ADS1234 Channel 1 for loadcell [bipolar] Channel 2 for pressure senosr[unipolar]
Gain : Both channels has same gain 128
Problem Statement : When we read Loadcell at channel 1 we get proper sequnce of DRDY ,SCLK, and Data then DRDY high at 25th clock and data read is proper. as per datasheet.But after switching the channel [2] for pressure sensor below sequence has been observerd:
Switch channel [1 to 2nd] -> add 50 microsecond delay -> DRDY High for 50 msecond -> DRDY Low -> DRDY High for 20 msecond -> Data [with 24 clocks] + 25th clock + DRDY high.
So queries are
1. Is that whether above sequence is OK ?If not then why DRDY pin is high for second time[20ms]
2. Can we use combination of bipolar and unipolar inputs on same ADC.
Harsh Goel
Bosch India
+91-9886001802