Hello,
I need to use the ADS130E08 to measure 3 phase power. Each phase would need to be deferentially measured in reference to ground. Figure 42 shows a diagram of how to wire in a line relative to Neutral.
Does the voltage divider (R2/(R1+R2)) need to make sure that the voltage across the top R2 is at a maximum of 4 volts?
Does the neutral line also need the same division values of resistors as the power line?
When connecting three phases of power to the same chip, do I need to have a separate set of input resistors (6 resistors) per phase?
Also, all three phases would connect to the OPAMPOUT pin in parallel with each other, correct?
Thank you for your help in advance!