Hello,
I plan to use multiple DAC161S997 in one project to generate multiple 4-20mA outputs. Before I start the design, two DAC161S997EVM were purchase to test if any issues. I did some tests. The loop+ power input was shared for two EVM boards. One issue I found is that two 4-20mA outputs are not independent. If I changed one output, the other is also changed proportional (looks like a proportional current mirror). If I seperate loop+, they are independent. What do you think the issue is?
Thanks in advance.