Hi,
Our customer has some questions about ADS7952.
*Q1
What does 「Absolute input range」 parameter mean ? In case of Range2, even if we break the spec min=-0.2 V, max=2*VREF + 0.2 V, I beleive the davice doesn't have damage. Because the spec isn't ABSOLUTE MAXIMUM RATINGS.Is my understanding correct?
*Q2
Could we input 4Vmax at AINP pin for Range1 mode[default] ? Customer is going to set VA=5V , Vref=2.048V.
◆ELECTRICAL CHARACTERISTICS
◆ABSOLUTE MAXIMUM RATINGS
Best Regards,
Kato