Hi,
Did anybody tried to drive ADS1274/1278 with an standard SPI supportive MCU ?
here is my question:
1: should I use Master SPI or Slave SPI mode in MCU side?
2: in SPI communication, we have MISO/MOSI/SS/SCLK (4wires) .. what are these pins in ADS chips?
3: what is the maximum Bit rate that I can use in data transmission ?
4: how much delay do I need to have between /(DRDY) going low to first transition on SCLK?
Thanks
M