Hello,
I have the ADS131E08 EVM attached to an MSP430F5418. I need to read the A2D using SPI - UCSB0SPI.
The wiring is as follows:
MSP430 f 5418 | Desc. | EVM Board |
P3.0 | SPI_CS | JP8.2 |
P1.1 | SPI_Start | JP9.2 |
P3.1 | SPI_IN | J1.11 |
P3.2 | SPI_OUT | J1.13 |
P1.2 | SPI_DRDY | J1.15 |
P3.3 | SPI_CLK | J1.3 |
GND | J1.18 |
I'm trying to read the registers of the ADS131
unsigned char TempData[20]; //****************************************************************************** // ADS131/MSP430x5418 Demo - ADS_131 to MSP430 communication via SPI // // // Description: Use of the MSP430 USCI A0 peripheral for setting up and // communicating to the ADS_131 // // // // MSP430x5418 // ------------------ // /|\| | // | | | // --|RST P3.2|<-- MISO (DOUT) // | | // | P3.1|--> MOSI (DIN) // | | // | P3.3|--> SCLK // | | // | P1.2|<-- INT (DRDY) // | | // | P3.0|--> CS // // R. Benjamin // Texas Instruments Inc. // May 2013 // //****************************************************************************** //+-----------------------------------------------------------------------------+ //| Source: main.c, v1.0 2013/05/28 | //------------------------------------------------------------------------------+ #include <msp430f5418.h> #include "ADS1220.h" // Function declarations void Init_StartUp(void); void SPIinit(void); // Global variable int dflag = 0; long tData[8][500]; /*----------------------------------------------------------------------------+ | Main Routine | +----------------------------------------------------------------------------*/ void main(void) { int idx = 0; WDTCTL = WDTPW + WDTHOLD; // Stop watchdog timer Init_StartUp(); // Initialize device ADS_131_Init(); // Initializes the SPI port pins as well as control ADS_131_Config(); // Set base configuration for ADS1x20 device } //main() /*----------------------------------------------------------------------------+ | System Initialization Routines | +----------------------------------------------------------------------------*/ // Initializes the clocks. Starts the DCO at USB_MCLK_FREQ (the CPU freq set with the Desc // Tool), using the REFO as the FLL reference. Configures the high-freq crystal, but // doesn't start it yet. Takes some special actions for F563x/663x. void Init_Clock(void) { P5SEL |= 0x0C; P5DIR |= BIT4+BIT5; UCSCTL1 = DCORSEL_6; UCSCTL2 = FLLD_1+1; UCSCTL3 = SELREF__XT2CLK; UCSCTL6 = XT2DRIVE1; // Start the FLL, which will drive MCLK (not the crystal) //Init_FLL(USB_MCLK_FREQ/1000, USB_MCLK_FREQ/32768); //Init_FLL(USB_MCLK_FREQ/1000, USB_MCLK_FREQ/12000000); UCSCTL4 = SELA_4 + SELS_4 + SELM_4; // ACLK=TX2 SMCLK=TX2 MCLK=TX2 P2SEL |= BIT2; P2DIR |= BIT2; __bis_SR_register(GIE+OSCOFF); } //---------------------------------------------------------------------------- void Init_Ports(void) { // Initialization of ports all unused pins as outputs with low-level // set all ports to low on all pins P1OUT = 0x04; P1DIR = 0xFF; P2OUT = 0x00; P2DIR |= 0x3F; P3OUT = 0x00; P3DIR |= 0x07; P4OUT = 0x00; P4DIR |= 0xFF; P5OUT = 0x00; P5DIR |= 0x33; P6OUT = 0x00; P6DIR = 0xFF; } //---------------------------------------------------------------------------- // Sets the USCI SPI peripheral to use B0 void SPIinit(void) { UCB0CTL1 |= UCSWRST; // Hold peripheral in reset UCB0CTL0 = UCMST + UCSYNC + UCMSB; // SPI master, synchronous UCB0CTL1 = UCSSEL_2 + UCSWRST; // Use SMCLK for bit rate clock and keep in reset UCB0BR0 = 12; // SMCLK/12 = SCLK (2MHz) UCB0CTL1 &= ~UCSWRST; // Release peripheral for use } //---------------------------------------------------------------------------- void Init_StartUp(void) { __disable_interrupt(); // Disable global interrupts Init_Ports(); // Init ports (do first ports because clocks do change ports) // SetVCore(3); // USB core requires the VCore set to 1.8 volt, independ of CPU clock frequency Init_Clock(); SPIinit(); __enable_interrupt(); // enable global interrupts } void ADS_131_Init(void) { P3SEL |= ADS1220_DIN + ADS1220_DOUT + ADS1220_SCLK; P1SEL &= ~(ADS1220_DRDY); P3SEL &= ~(ADS1220_CS); // define initial states P3OUT |= (ADS1220_CS); // CS is really 'not' CS, so it should be disabled high // define inputs P1DIR &= ~(ADS1220_DRDY); // DRDY is an input to the micro P1IES |= ADS1220_DRDY; // and should be used as an interrupt to retrieve data // define outputs P3DIR |= ADS1220_CS; return; } void ADS_131_AssertCS( int fAssert) { if (fAssert) P3OUT &= ~(ADS1220_CS); else P3OUT |= (ADS1220_CS); } void ADS_131_SendByte(unsigned char Byte) { char dummy; while(!(UCB0IFG & UCTXIFG)); UCB0TXBUF = Byte; while(!(UCB0IFG & UCRXIFG)); dummy = UCB0RXBUF; } unsigned char ADS_131_ReceiveByte(void) { unsigned char Result = 0; while(!(UCB0IFG & UCTXIFG)); // Make sure nothing is currently transmitting UCB0TXBUF = 0xff; // Send out NOP to initiate SCLK while(!(UCB0IFG & UCRXIFG)); // Wait until all data is transmitted (received) Result = UCB0RXBUF; // Capture the receive buffer return Result; } void ADS_131_ReadRegister(int StartAddress, int NumRegs, unsigned char *pData) { int i; // assert CS to start transfer ADS_131_AssertCS(1); // send the command byte // Register Read Commands // RREG | Read n nnnn registers starting at address r rrrr | 001r rrrr (2xh) | 000n nnnn // // r rrrr = starting register address for read and write opcodes. // n nnnn = number of registers to be read or written – 1. // For example, to read or write three registers, set n nnnn = 0 0010. ADS_131_SendByte(0x20 | (StartAddress & 0x1F)); ADS_131_SendByte((NumRegs-1) & 0x1F); // get the register content for (i=0; i< NumRegs; i++) { *pData++ = ADS_131_ReceiveByte(); } // de-assert CS ADS_131_AssertCS(0); return; } // ADS1220 Initial Configuration void ADS_131_Config(void) { ADS_131_ReadRegister(0, 1, &(TempData[0])); ADS_131_ReadRegister(0, 1, &(TempData[1])); ADS_131_ReadRegister(0, 1, &(TempData[2])); ADS_131_ReadRegister(0, 1, &(TempData[3])); ADS_131_ReadRegister(0, 1, &(TempData[4])); }
Attached is the code I'm using to setup the SPI and registers. I'd appreciate any help.
Thanks,
Mechi
unsigned char TempData[20]; //****************************************************************************** // ADS131/MSP430x5418 Demo - ADS_131 to MSP430 communication via SPI // // // Description: Use of the MSP430 USCI A0 peripheral for setting up and // communicating to the ADS_131 // // // // MSP430x5418 // ------------------ // /|\| | // | | | // --|RST P3.2|<-- MISO (DOUT) // | | // | P3.1|--> MOSI (DIN) // | | // | P3.3|--> SCLK // | | // | P1.2|<-- INT (DRDY) // | | // | P3.0|--> CS // // R. Benjamin // Texas Instruments Inc. // May 2013 // //****************************************************************************** //+-----------------------------------------------------------------------------+ //| Source: main.c, v1.0 2013/05/28 | //------------------------------------------------------------------------------+ #include <msp430f5418.h> #include "ADS1220.h" // Function declarations void Init_StartUp(void); void SPIinit(void); // Global variable int dflag = 0; long tData[8][500]; /*----------------------------------------------------------------------------+ | Main Routine | +----------------------------------------------------------------------------*/ void main(void) { int idx = 0; WDTCTL = WDTPW + WDTHOLD; // Stop watchdog timer Init_StartUp(); // Initialize device ADS_131_Init(); // Initializes the SPI port pins as well as control ADS_131_Config(); // Set base configuration for ADS1x20 device } //main() /*----------------------------------------------------------------------------+ | System Initialization Routines | +----------------------------------------------------------------------------*/ // Initializes the clocks. Starts the DCO at USB_MCLK_FREQ (the CPU freq set with the Desc // Tool), using the REFO as the FLL reference. Configures the high-freq crystal, but // doesn't start it yet. Takes some special actions for F563x/663x. void Init_Clock(void) { P5SEL |= 0x0C; P5DIR |= BIT4+BIT5; UCSCTL1 = DCORSEL_6; UCSCTL2 = FLLD_1+1; UCSCTL3 = SELREF__XT2CLK; UCSCTL6 = XT2DRIVE1; // Start the FLL, which will drive MCLK (not the crystal) //Init_FLL(USB_MCLK_FREQ/1000, USB_MCLK_FREQ/32768); //Init_FLL(USB_MCLK_FREQ/1000, USB_MCLK_FREQ/12000000); UCSCTL4 = SELA_4 + SELS_4 + SELM_4; // ACLK=TX2 SMCLK=TX2 MCLK=TX2 P2SEL |= BIT2; P2DIR |= BIT2; __bis_SR_register(GIE+OSCOFF); } //---------------------------------------------------------------------------- void Init_Ports(void) { // Initialization of ports all unused pins as outputs with low-level // set all ports to low on all pins P1OUT = 0x04; P1DIR = 0xFF; P2OUT = 0x00; P2DIR |= 0x3F; P3OUT = 0x00; P3DIR |= 0x07; P4OUT = 0x00; P4DIR |= 0xFF; P5OUT = 0x00; P5DIR |= 0x33; P6OUT = 0x00; P6DIR = 0xFF; } //---------------------------------------------------------------------------- // Sets the USCI SPI peripheral to use B0 void SPIinit(void) { UCB0CTL1 |= UCSWRST; // Hold peripheral in reset UCB0CTL0 = UCMST + UCSYNC + UCMSB; // SPI master, synchronous UCB0CTL1 = UCSSEL_2 + UCSWRST; // Use SMCLK for bit rate clock and keep in reset UCB0BR0 = 12; // SMCLK/12 = SCLK (2MHz) UCB0CTL1 &= ~UCSWRST; // Release peripheral for use } //---------------------------------------------------------------------------- void Init_StartUp(void) { __disable_interrupt(); // Disable global interrupts Init_Ports(); // Init ports (do first ports because clocks do change ports) // SetVCore(3); // USB core requires the VCore set to 1.8 volt, independ of CPU clock frequency Init_Clock(); SPIinit(); __enable_interrupt(); // enable global interrupts } void ADS_131_Init(void) { P3SEL |= ADS1220_DIN + ADS1220_DOUT + ADS1220_SCLK; P1SEL &= ~(ADS1220_DRDY); P3SEL &= ~(ADS1220_CS); // define initial states P3OUT |= (ADS1220_CS); // CS is really 'not' CS, so it should be disabled high // define inputs P1DIR &= ~(ADS1220_DRDY); // DRDY is an input to the micro P1IES |= ADS1220_DRDY; // and should be used as an interrupt to retrieve data // define outputs P3DIR |= ADS1220_CS; return; } void ADS_131_AssertCS( int fAssert) { if (fAssert) P3OUT &= ~(ADS1220_CS); else P3OUT |= (ADS1220_CS); } void ADS_131_SendByte(unsigned char Byte) { char dummy; while(!(UCB0IFG & UCTXIFG)); UCB0TXBUF = Byte; while(!(UCB0IFG & UCRXIFG)); dummy = UCB0RXBUF; } unsigned char ADS_131_ReceiveByte(void) { unsigned char Result = 0; while(!(UCB0IFG & UCTXIFG)); // Make sure nothing is currently transmitting UCB0TXBUF = 0xff; // Send out NOP to initiate SCLK while(!(UCB0IFG & UCRXIFG)); // Wait until all data is transmitted (received) Result = UCB0RXBUF; // Capture the receive buffer return Result; } void ADS_131_ReadRegister(int StartAddress, int NumRegs, unsigned char *pData) { int i; // assert CS to start transfer ADS_131_AssertCS(1); // send the command byte // Register Read Commands // RREG | Read n nnnn registers starting at address r rrrr | 001r rrrr (2xh) | 000n nnnn // // r rrrr = starting register address for read and write opcodes. // n nnnn = number of registers to be read or written – 1. // For example, to read or write three registers, set n nnnn = 0 0010. ADS_131_SendByte(0x20 | (StartAddress & 0x1F)); ADS_131_SendByte((NumRegs-1) & 0x1F); // get the register content for (i=0; i< NumRegs; i++) { *pData++ = ADS_131_ReceiveByte(); } // de-assert CS ADS_131_AssertCS(0); return; } // ADS1220 Initial Configuration void ADS_131_Config(void) { ADS_131_ReadRegister(0, 1, &(TempData[0])); ADS_131_ReadRegister(0, 1, &(TempData[1])); ADS_131_ReadRegister(0, 1, &(TempData[2])); ADS_131_ReadRegister(0, 1, &(TempData[3])); ADS_131_ReadRegister(0, 1, &(TempData[4])); }