Hi,
I am running a DAC8760 on 0 and 12V rails. On the 0-10V output there is an offset of approx 10.5mV at Zero.
- I guess that running on dual rails is the only way of obtaining a true 0V output?
- Is there any issue with using asymmetric rails e.g 12V and -5V.
- Can you recommend an inverter to generate the negative rail from either 12V or 5V