Hi All,
I was reading the datasheet of the ads1274 data converter for a new design and I noticed that the voltage reference input is a differential input, but when I look to the maximum ratings it's stated that the input range for the reference input is:
VREFN = AGND -0.1V (MINIMUM) and VREFN = AGND +0.1V (MAXIMUM)
Shouldn't the maximum be AVDD+0.1V? If I take a look at the Figure 70 - Equivalent Reference Input Circuity, both reference inputs are clamped to AGND and AVDD which would indicate that the maximum rating is:
VREFN = AGND -0.1V (MINIMUM) and VREFN = AVDD +0.1V (MAXIMUM)
Could someone please verify this because I would like to use a 2.5V full differential buffered voltage reference, with 2.5V VCOM as offset.
Best regards,
Tjarco Boerkoel
the Netherlands