I am referring to the
- Application note "ECG Implementation on the TMS320C5515 DSP Medical Development Kit (MDK) with the ADS1298 ECG-FE” from the following link: http://www.ti.com/lit/an/sprabj1/sprabj1.pdf
- User guide “ADS1298 ECG-FE Front End Performance Demonstration Kit”. http://www.ti.com/lit/ug/sbau171c/sbau171c.pdf
They will be henceforth referred to as item 1 and 2 respectively. I am some queries regarding the differences between these two items.
For instance, I understand that item 1 consists of the ADS1298ECG-FE and the TMS320C5515 DSP evaluation module. These two can be configured together to perform as described in the application note, with the DSP software that can perform various ECG-related functions.
On the other hand, I understand that item 2 consists of the ADS1298ECG-FE and the MMB0 motherboard. The MMB0 acts as an interface between the ADS1298ECG-FE and the PC.
Thus my queries:
- What are the differences between setups in item 1 and 2 respectively, apart from the ones I've mentioned?
- What else can the MMB0 do? I note that it has a TMS320VC5509A digital signal processor on it. Can it be used to do signal processing like the one TMS320C5515 in item 1?
- If yes, can I program my own functions to perform the ECG-related features like stated in item 1? (Eg. Data acquisition through ADC, Lead-off detection, DC signal removal)
I am planning to purchase the ADS1209ECG-FE for an ECG project and would require a digital signal processor to implement my functions. As such I am unsure of the difference between these two setups.
Thank you for your help.
Regards,
Aslam