Hello,
I am using the ADS1258 EVM (acquisition board) to record 4 channels simultaneously, and i am using the the ADCpro software to record the data.
My switch delay time is 0 micro seconds.
According to the ADCpro manual: "the number of samples taken depends on the block size set in the test plug-in and/or the number of points set to record in the data recorder." in addition to that it tells us that "the max block size for any test is 1 048 578 samples per channel." but for some reason i am not being able to obtain more than 60 000 samples per channel. My data rate is 5.8342kHz
we are using the data recorder in ADCpro and saving it to a file
My main goal is to at least obtain 2 minutes of data using 4 channels, each recording (a minimum of 1 000 000 samples per channel) simultaneously.
Thank you,
Andres