Hi, all!
My customer has questions about ADS1672 offset error.
When AVDD was changed from 4.75 V to 5.25 V , the offset was varied by about 250 uV.
The test condition is as follows;
- Test circuit is almost the same as Figure 39. Basic Analog Signal Connection of Page 26.
- Low-Latency, Fast-Response
- Sampling frequency: 125 kHz
- DVDD = 3.3 V
- fck = 20 MHz
- Vref =+3 V
- Rbias = 7.5 kΩ
- Input level: AINP = AINN = 2.5 V
1. Meaning of the PSSR is a variation of Full scale with respect to the change in the power supply voltage.
Is it right?
Is PSSR is related with OFFSET error?
2. How much is change of OFFSET to change of AVDD?
3. Is the 250uV offset change the performance of ADS1672?
Regards,
Toshi