Hi,
I am using two ADS1278s daisy chained on a board and I don’t have the AGND and DGND connected on the board, it is happening somewhere outside. Oddly though, I still get only 5 ohms between AGND and DGND when I expect to see at least 1Mohm. If I pull out the ADCs, then AGND and DGND are open. So I tried ohming the pins of the ADS1278 stand-alone and I don’t see a 5 ohms path between AGND and DGND. Any idea whats going on? In my system the grounds are connected together on a separate power section board.