Hello,
I'm trying to use the ADS1278 with a data rate of 40kHz with an f_mod of 2.56 MHz, I'm using the THS4531A to drive it. The datasheets suggests putting a 50-ohm resistor at the input of the ADC, followed by a 2.2nF capactitor. I'm concerned by the attenuation from these resistors, using the diagram in Figure 69 of the datasheet, it looks like I would get about 0.27% of error. However, there's nothing on how this impedance might change over frequency or input voltage; is this something that can calibrated out with a simple linear calibration?
Doesn't it defeat the purpose of using such a high bandwidth driver if you have an RC filter like that behind it? Would using a smaller series resistor improve accuracy, or would it make it ring more?